What's New in Confirm?
Confirm v26.20 and ConfirmConnect™
We are delighted to announce that the latest release of our industry leading Enterprise Asset Management solution, Confirm® is now available in the OnDemand Production and Test Environments.
The enhancements since the last release include:
Supported Technology and Platforms
Support Withdrawal Notice
With effect from Confirm v26.20, the Mapping Interface for ESRI ArcMap 10.2.2 to 10.8.1 and ESRI ArcGIS Pro 2.4 to 2.9.8 will cease support. This will be replaced by the ArcGIS 2-Way Sync.
General Functionality
Mendix Custom Forms in Confirm Web
Mendix Custom Forms can now be launched directly from the Asset, Enquiry, Defect, and Job screens in Confirm Web.
A new Apps & Links section brings together Product Integrations, application links, and Custom Forms under a single, organised menu.
Customisable Search Columns
Users can now add, remove, and reorder columns to customise search results according to their requirements, with changes reflected immediately on screen. Results can also be sorted by any
displayed column, making it easier to prioritise and analyse data. Additionally, users can export up to 1,000 records in a single action directly from the search page.
Open Geospatial Consortium is now supported in confirm GIS
Confirm Web GIS now supports OGC connections, allowing users to integrate and display map layers from external, standards-based GIS services WMS, WFS, and WMTS.
New OGC Connection features enable Confirm Web GIS to connect with external GIS services, providing access to diverse map layers and geospatial data.
ConfirmConnect®
Browsers
ConfirmConnect is now fully supported on Chrome, Edge, Firefox and Safari.
Android Devices
Android 16 is now supported.
Ability to open Defects directly from What's Going On Here Map
Users can now view full Defect record details directly by selecting the Defect record on the map.
Users can also supersede Defects (where permitted), save changes as a draft, or submit updates immediately without leaving the map view.
The Defect icon on the map dynamically reflects the current status of the Defect.
NOTE Access is controlled by existing security permissions.
Add Defect Search
Users can now search and filter Defects from the Defects list using search criteria such as number, type, description, or location when linking an Enquiry or carrying out Inspections/Surveys in ConfirmConnect.
This allows for quick and efficient identification of the correct Defect, eliminating the
need to scroll through long lists.
Reduced White Space in Attributes Section
ConfirmConnect now provides a concise and cleaner screen layout with reduced white space in the Attributes section, enabling Inspectors to view more information at a glance with less scrolling.
Confirm Web Interface
Advanced Filtering for Features: Filter by Attributes
Confirm Web now supports advanced filtering of Feature records using attribute values such as pick lists, free text, numeric fields, and dates, enabling users to quickly and accurately find specific records.
Advanced Filtering for Enquiry, Defect and Job: Filter by Attributes
Confirm Web now enables advanced filtering of Enquiry, Defect, and Job records using attribute values. These include pick lists, free text, numeric fields, and dates, allowing users to quickly and accurately identify specific records.
Confirm Enterprise Browser Engine Upgrade
Confirm Enterprise now uses CefSharp to render embedded Confirm Web screens, delivering a more secure, stable, and seamless experience. By replacing the outdated CefGlue component with modern technology, it enhances security, resolves existing issues for improved reliability, and reduces maintenance effort.
Release Notes 07.21.2026
Rebranding to Siemens Software
Brightly is now Siemens. Same world-class software, new look and feel.
From v22.10, the Confirm product suite has been rebranded to align with Siemens.
This update introduces Siemens branding across the application, replacing previous Brightly Software branding within customer-facing screens and supporting documentation.
The support email displayed in help documentation reflects the new Siemens address for the Support Team.
As part of this transition, support contact information has also been updated, and help documentation now reflects the Siemens Support Team email address.
This rebranding does not affect product functionality and is intended to provide a consistent experience across the Siemens Confirm software offerings.
Confirm v26.1 and ConfirmConnect™
v26.1 – OnDemand US Production and Test Complete
We are delighted to announce that the latest release of our industry leading Enterprise Asset Management solution, Confirm® is now available in the OnDemand Production and Test Environments.
The enhancements since the last release include:
Streamlined Web Operations (Confirm Web Interface)
We've significantly expanded the capabilities available directly in the Confirm web interface, reducing the need to switch applications and boosting your productivity:
-
Improved Web Navigation: Users can navigate large data sets more easily with clearer pagination controls on the search results in the Confirm Web interface, enabling faster review and more accurate data handling.
-
Enhanced Data Descriptions: Users can store longer, more descriptive operational attribute names and values, improving data clarity and consistency across teams.
-
Batch Payment Processing Preview: Users can preview batch payment checks and authorisations, improving accuracy and confidence before payments are created.
-
Web Based User Administration: Users can manage users, reset preferences, generate API keys, and copy permissions, simplifying day to day administration.
-
Clearer Defect Context: Users can clearly see Defect type descriptions and references on Defect screens, reducing errors and improving understanding during review.
-
Web First Asset & Regime Management: Users can create Enquiries, Defects, Jobs, and manage regimes directly from the Feature screen, improving efficiency and supporting Web first workflows.
-
Enhanced Reporting Drill Down: Users can drill from dashboards directly into Orders, Payments, Inspections, and Street Works, enabling quicker access to detailed operational insight.
-
Meter Based Maintenance Support: Users can now perform maintenance activities based on meter based and time/meter based readings, improving scheduling accuracy and reducing manual effort.
-
Reusable Comment Library: Users can insert pre defined comments when creating Enquiries, enabling faster responses and more consistent customer communications.
-
Inspection Route Editing in Web: Users can add, edit, and remove Inspection Route Features, reducing reliance on legacy tools and speeding up inspection setup.
-
Refined Enquiry Prioritisation: Users can filter Enquiries by outstanding or completed status, allowing quicker prioritisation of work and improved service responsiveness.
-
Order Management in Web: Users can create and manage Job Orders entirely in the Confirm web interface, including Job associations, enabling simpler maintenance planning without switching systems.
Empowering Field Teams with ConfirmConnect
For our colleagues in the field, ConfirmConnect gets even smarter:
-
Smarter Mobile Mapping: Users benefit from automatic map refresh and spatial search in ConfirmConnect, enabling faster and more reliable visibility of nearby work while on the move.
-
Improved Defect Identification: Users can view Defect numbers directly in lists and on map icons in ConfirmConnect, supporting faster and more accurate Defect selection.
-
Faster Defect Creation: Users can create new Defects more quickly via a prominent Add Defect action in ConfirmConnect, reducing time on site and streamlining inspection workflows.
-
Job Completion Visibility on Maps: Users can see Job completion dates directly in map searches within ConfirmConnect, improving visibility of completed work and reducing duplicate actions.
-
Enhanced Document & Photo Viewing: Users can view linked documents and larger photo previews at a glance in ConfirmConnect, improving situational awareness with less navigation effort.
-
Clearer Mobile Settings Navigation: Users can manage preferences more easily with clearly separated Settings and About pages in ConfirmConnect, reducing confusion and simplifying configuration.
-
Accurate Asset Geometry in Surveys: Users can view precise asset geometries during Route Surveys in ConfirmConnect, enabling more accurate inspections and higher confidence in recorded data.
-
Inline Defect Creation During Surveys: Users can create and complete Defects without leaving the survey screen in ConfirmConnect, resulting in faster inspections and improved data completeness.
-
Cleaner Defect Data on Supersede: Users automatically retain only relevant attributes when Defect types change in ConfirmConnect, ensuring higher data quality and more reliable reporting.
-
Integration & Compliance with Street Manager
-
Prevents duplicate non-compliance records by prompting users to link existing NCs when creating new inspections for the same permit. This improves data consistency between Confirm and Street Manager, reducing rework and mitigating compliance risks.
-
Streamlining multi trench Permit processing by generating a single inspection and non compliance record, reducing duplication and simplifying data management. This ensures alignment with Street Manager workflows, improving data accuracy, reporting, and compliance.
We are confident that these enhancements will significantly boost your productivity and provide a more seamless experience across the board. We're committed to continuously improving Confirm to meet your evolving needs. We encourage you to explore these new features and discover how they can empower your daily work. If you have any questions or need assistance, our support team is always here to help!
For further information on the items above, please view the attached “What’s New v26.0 & v26.1” documentation. A webinar will be conducted soon to demonstrate and explain these functionalities.
Please review the ConfirmConnect Release Notes for details of changes included with this release. There is no container update for this release. Please ensure all ConfirmConnect users complete any draft tasks, sign out and sign in to upgrade their devices.
If you encounter any problems with your upgrade, please contact our Technical Support team at confirm.support@brightlysoftware.com.
Archived Release Notes
Click here to view previous releases that have been deployed to Confirm.